AS6 - supported hardware - c30/c70

Hi there,

Any estimation, when the power panel c30 series will be supported?

According to the documentation the c70 series won’t be supported. This is set in stone?

Many thanks,
Torsten

The C30 is supported.
The C70 is not supported.

I’m somehow unable to find any c30 hw files

The C30 hardware files and AR are contained in the AS V6.0.2.177, which is released yesterday.

Thanks Corne, ok the issue is that we have a customized C30 panel which isnt supported (yet). Hope it will be added soon since I’m eager to try out AS6 ^^

I also could not find customized C30 panels, only these ones:
image

customized c30 will be not automatically added to AS6. You have to ask B&R and its respective department for that.