Automation Runtime version V2.52

Hi experts,

I’m looking for the Automation Runtime version V2.52 for the Power Panel 4P3040. But i can’t find it out in any Automation Studio V2.x, V3.x package. Please kindly share it if you have.

Thanks in advance!

Hello Huynh,

More of the part number is needed to get the correct hardware upgrade. The standard part is 4P3040.00-490 but there are also plenty of custom Power Panel 40s with part number 4P3040.00-Kxx. If you look up “4P3040.00 upgrade” on our website there are various hardware upgrades for AS 2.6 and 3.0. As a note some of these upgrades can only be seen if you are logged in.

-Ryan

Hi Ryan,

Thanks for your reply. But, I can’t find out this Automation runtimer version even I’ve already logged in. There are only some common AR version like 2.95, 2.96. So, I think this AR version is customized for some customer, and not public. If you have any idea, please feel free to share it.

-Phi

Hi @tranphi1310,

V2.52 for SG3 systems (Motorola-based PLCs) was part of the final Automation Studio 3.0.90 installation package.
I’ll try to upload the single AS3 uprade in a 2nd post, but I’m not sure if the upload is accepted by the forum system - so here’s also the screenshot where to find it inside the complete Automation Studio 3 package:

(AS_3.0.90.37_UP19)

Best regards!

As mentioned, here’s the upload of the singe AS3 upgrade package for V2.52

AR_V2.52_AS3.zip (5.1 MB)

Hi Alexander,

Thanks a lot for your prompt support. It helps me.

Have a nice day!