Automation PC 910 - Problem after BIOS Downgrade

Hello everyone,

I downgraded the BIOS of an Automation PC 910 from version 1.23 to version 1.22 and after the automatic reboot triggered by the update script, I never got an image signal back. The problem is that the USB ports also seem to be inactive after this restart (no keyboard recognized). When power is given to the APC, the power LED lights up red for a brief moment and then green, just like on a normal startup.

There is no activity from the HDD LED either.

Can the PC be saved somehow or did the contents of the BIOS memory get destroyed after the downgrade?

Last but not least, the procedure went on smoothly and I got the message in the end that the BIOS was flashed successfully, nothing went wrong during the procedure.

I am grateful for any help or feedback provided.

Hardware details:

Board: TS17-00
BIOS: 1.23 downgraded to 1.22

Issue was solved by flashing new BIOS. Assumption is that either upgrade was not 100% or flash is defective. Downgrade from 1.23 to 1.22, should be possible and it is perfectly fine to do that.

Tip for next time: you should try all USB interfaces including the one on the front of APC. If you find one that is active you can try blind BIOS reset to default as we discuss together here Link or use repair channel