Automation Studio project files (*.apj) contain information about the version with which the project was created or edited.
If you are working with several Automation Studio installations, the project should always be opened with the correct version.
It can happen that the standard programme for opening these (*.apj) is lost or incorrectly changed in Windows.
To open the file directly with the correct version again, the AutomationStudioLauncher must be specified as the default tool and not Automation Studio directly. The launcher opens the apj file, checks the version used and opens it.
This means that the default programme for apj files in Windows does not have to be the pg.exe itself, but the AutomationStudioLauncher under the following path:
<AS-Installationspfad>/BrAutomation/AsTools/AutomationStudioLauncher.exe