Border problem in dialog with radius

I am using dialog windows and when I set the border then the contetnt don’t show over full place. There is still some transparent space. Tested variants:

  • No border + no radius: OK
  • Border + no radius: OK
  • No border + radius: OK
  • Border + radius: Problem

I test also different version of border for header and body, but not help. Also try differnt type of sizeMode.

Any suggestions?
AS 6.7, mappView 6.8

is it problem only in AS editor or in browser as well? what about padding configuration?

It’s from browser. In AS editor are not the tool to show the full dialogs.

Padding is not posibble in dialog.

On panel it’s look good, but the problem is on PC. Maybe the another resolution or resizing the visu? But everthing else is good.

Coulld be pixeling drawing issue?

Try this:

  • Set browser zoom to 100%
  • Check Windows DPI / display scaling on the affected PCs
  • Test with a different browser
  • If possible, overlap the content by 1 px under the rounded border as a workaround

@NovotnyJ, any update there?

I am trying solve another problem, but I will be back :saluting_face: