We encountered an issue yesterday about ACCS with status not ready and after check the reason we found BR runtime with Cfgcode 15 but in normally status with Cfgcode 31.Check the hardwar configuration BR (ip adress and name are correct)but when change the config file the issue solved ,but now I wanna know what the reason for this issue and Cfgcode change to 15(incorrect status)
Welcome to our Community!
We’re going to need some more information before anyone can help you. “Cfgcode” isn’t a term I recognize, and the error numbers provided by B&R components are typically more than two digits. Where are you seeing these error messages? Is it within Automation Studio or another software?
Also, what is ACCS?
ACCS(Automatic crane control systems) the pc or I mean plc to control and management the subsystem
It sounds like the B&R PLC is part of a larger system and that the overall system controller is giving you error codes. If this is the case, you’ll have to check with the developer of this system to see what these error codes mean and hopefully get B&R specific error codes.
I see you’ve marked my last reply as the solution. If you have any more information you’d like to share or questions you’d like to ask later, let us know!