C80 in Web mode but with VNC access?

Hi,
I need to use C80 Panel in web mode (with mappView), but also to have access trough vnc client for remote assistance.
Is it possible to do it?

mapp View has a VNC widget. So, if your VNC server is on a network that can be accessed from the C80, it should work.

I explained myself wrongly.

I have a C80 with mappView visualization.
I want to connect to C80 from remote location and access it with VNC client to see wich pages and buttons the operator use, or to change page and teach the operator.

In conclusion, I need a VNC server on C80, like others B&R Panel.

it doesn’t make sense from my point of view. If you have a remote connection to the C80, you can access mappView remotely as well. You do not need VNC for that. You can even create a special service mappView visualization for this if you do not want to access the primary main visualization.

It make sense for our help desk and assistance.
Sometime, we need to see what buttons the operator press, and in which page he is. Or the opposite: we need to teach to operator which button press or in which page there is the data that he is looking for.

ok…now I see your use case. C80 is hypervisor system, but GPOS part is not open for user application. You need hypervisor system where GPOS (Windows/DEBIAN) can be accessed/configured by user e.g. ppc2200 would be probably equivalent to your C80. On this system you can use e.g. DEBIAN as a GPOS, install VNC server and this will meet your requirement.

Hi Simone, I marked one of the replies as a solution/answer to your question. But feel free to mark the one that helped you the most or continue the discussion if more information is needed.

Ok, thank you for your help

Hi,
this is the solution for my problem: