Circuit of The accelerometer and the module X20CM4800X

Hello guys,
I would like to ask you for clarification regarding the connection between my accelerometer and the X20CM4800X module.

The accelerometer cable I am currently using has only two wires:

  • Red wire: connected to IEPE+ / signal
  • Blue wire: connected to 0V
  • Additionally, there is a grey shielding wire that I connected to close the circuit.

However, according to the X20CM4800X datasheet, the module expects a 3-wire connection: IEPE+, IEPE−, and shield.


The issue is that the module indicates a broken wire.
I would like to know if it is possible to connect my accelerometer to the X20CM4800X module, and if so, how should I proceed to do it properly?


Unfortunately, I have no knowledge of this type of measurement, but I’ll just try to understand the documentation.

According to Wikipedia this kind of sensors need a power supply, which this module can provide (but can be switched off by application).

  • does the sensor work with the provided Milliamps ? (Datasheet)

  • then the technical data describe how the open circuit detection works:

so one can check the voltage.

-then I would still have concerns about the pin naming ‘GND’ instead of ‘IEPE-’. ‘GND’ implies that there is a grounding to the housing (?) whereas IEPE+/- expect a floating (groundless) sensor input.

This is the electrical data of my accelerometer.


my module provide 5mA/24VDC like a supply power.
and the accelerometer had an excitation voltage between 18-28VDC, constant current excitation between 2 and 20mA.
the probleme is that the module write that there is a Broken Wire and i don’t know the reason.

Thank you for helping.

what voltage did you measure between A+ and A- input of the module by using a multimeter ?

I didn’t try to mesure it, but based on this circuit is 5 mA.

what is the problem ? the pins are accessible according to your photo above :slight_smile:

the problem is the module give me a broken wire True as you see in the photo.
image
this is the circuit, and i activated the channel and the IEPE supply but without ny result.


e LED always blink

i mesured the voltatge between IEPE +/- and i found it equal 3.18 V and this is less than 8 v rocommanded by B&R and for the sensor it works between 8 and 12V. i don’t know why the module give me this voltatge and how i could resolve this problem.

I would guess your sensor requires more current than the maximum of 5.5 mA :frowning:. You could contact the manufacturer to be sure.