Hi, do I need an external power source to connectet sensor with 4-20mA output signal? It is not sure for me from the documentation.
Thanks.
Hi, do I need an external power source to connectet sensor with 4-20mA output signal? It is not sure for me from the documentation.
Thanks.
Hello,
The question was general about type of sensor. I thought from this wiring diagram, that I can connect 2wire sensor directly, for example VEGABAR82.
X20AI + to sensor + and X20AI - to sensor -.
But your answer means, this is not possible, I need external power source (Like you wrote, From anywhere where you get Supply). So, thanks
Hello,
There are 6 different versions of the Sensor available, as far as i understood. Each has its own set of pin connections. Only Version 4 Two-Wire HART has only 2 pins.
If you wan’t to use a HART Device, you must use a compatible AI-Card.
For example this X20AI2438 has HART Support.
Greetings
Michael
Thanks for your answer, it is clear now