I have a question, is it possible that CP0410 is no longer supported in version AS6.0? I can’t get mappView to work on this PLC! When I run the same project in a simulator or on another PLC, e.g. CP0483, mappview works normally.
X20CP0410 is still supported with Automation Studio 6.0. However the minimum suggested server hardware for mappView is X20CP0484.
Automation Help: mapp View hardware guidelines
With mapp View 5.x versions the minimum suggested was a X20CPx583. Due to Automation Studio / mapp versions 6 with increased cyber security when compared to versions 5 they also require more resources.
In my experience it has been possible to run 5.x with X20CP0410, even though it has fewer resources thang suggested. This is splitting hairs with the available RAM memory and does not leave much for the rest of the application.
You can check how much free RAM do you have left, for example via the System Diagnostics Manager.