Hi
I want to select Dark theme instead of white or grey theme in Automation studio.
Please clarify & help me how to select dark theme in AS software.
Hi
I want to select Dark theme instead of white or grey theme in Automation studio.
Please clarify & help me how to select dark theme in AS software.
Hi,
there’s no “official dark scheme”, but please have a look here (I assume you mean AS 4.12):
Best regards.
In addition to @alexander.hefner post the only official AS version with dark theme will be “AS Code”
Hello Alex,
trying to simply copy Editor.set into “C:\Users\kai_m\AppData\Roaming\BR\AS412 de” on a Win11 machine with AS4.12.6.106 isn’t working for me.
I have seen the older version of Editor.set (size 12kb) in the folder so I assume I copied the new file (which is way greater with 527kb) into the right folder. However no changing of the color theme after a restart of Auto Studio has been doing. Any idea why this file is ignored?
Hi @Transistorfips ,
I just did a quick test with my installation, which is AS 4.12.9.18 english (so my path is C:\Users\xxxx\AppData\Roaming\BR\AS412) → that worked as expected.
I’m surprised by the file size you mentioned (527k)? I can’t swear, but for me it sounds that it’s a much to big size for the normal editor.set.
The editor.set file in all settings I have is something around 12-15kByte, not more.
Additionally I checked the two files of the github repos linked above: they are in that range, too.
So could you please check your editor.set file, if it’s the / a right one? It should be a plain text file with XML content.
BG Alex
Something went south while copying the 527kb file from the github repo. However, it contained xml code. But you’re right, the size is abt. 14kb.
Then I c&p the code from automation-studio-editor-dark/Editor.set at main · boaz001/automation-studio-editor-dark · GitHub into the file. No effect. Did you tested the same file?
I then did a test by changing the fontsize in the editor and I have seen the timestamp of Editor.set changed to actual time.
I think the prob is somewhere else. Have to do deeper research.
Anyway, thanks for your help. I appreciate your fast response.
J.
There was some confusion about the user account on my local machine. Now it works flawlessly.
Thanks for your help, Alex.
Just not to leave it unanswered
I tested both files.
Happy to hear that it works now!
BG Alex