Delete projects in automation studio 4.12

Hello.

I understand that it’s a little ridiculous question, but I can’t find a tutorial on the answer.

  • What are the steps to follow to delete a project in AS4.12?

I have tried to delete the project but the message that I must have some active configuration but in this way I do not delete the project there is always some configuration left.

Any help is grateful.

Regards.

Hi Julián @electrofasa21
Did you closed your project in AS?
Then you could delete the directory directly from File Explorer.

Regards!

Close project or complete AS :slight_smile: and make sure that ArSim is also closed as well if you use it :slight_smile:

Hello.

-After closing my project, in order to delete it completely, do I just have to delete the .apj file and it will be deleted completely?

Regards.

No, not only *.apj file but everything what is in the same project folder.

Hola @electrofasa21

For example, I could delete the directory “mappVision-Demo-brdk” or the files inside this directory

Hello.

It has been clear to me, I understand that by deleting these files my projects will disappear from AS “projects”.

Thank you for your help.

Greetings :smiley:.