Hello together,
i have this error -1067313140 (Lag error higher than postion Error) at 6 of 9 of my identical Stepper Axis (MappMotion 6.3.1 )
In Configuration of Hardwaremodul 80SD100XD i can set Position Error but Error occurs independent of this Value.
But only at half of my Axis, other are working correctly with same settings. It´s confusing.
Anyone had this Error or any idea what can cause this. thanks
kovarj
(Jaroslav Kovar)
2
Update: The LagError occurs everytime i set PowerOn, because Motor is moving without any command. Direction seems to be random.
Update after TryAndError: Setting the controller to current not to position and current its is working correctly.
kovarj
(Jaroslav Kovar)
3
based on your update, I closed your topic as a solved. Feel free to update us with new findings