Hello,
I am doing a project conversion from AS 2.7 to AS 4.2.
The PLC is a 4PP420.1043-75 and till AS 3.0.90 all works fine.
Versions in AS 3.0.90 are:
AR R3.07
ACP10 2.39.2
VC 3.73.4
Now when I pass to AS 4.0.29.87, the rebuild all works fine but when I try to install on the PLC I have such error:
Transferring vcresman (UserROM, Vers: V4.06.2, 10.11.2016, 1543556 Byte, Path: C:\projects_40\17094_38\Binaries\Config1\PLC1\) …
Error : Error 9650 while transferring.: Library function not available (System GOT)
Versions in AS 4.0.29.87 are the following:
AR R3.07
ACP10 2.39.2
VC 4.06.2
Any possible reason? I an trying to find out AR 4.x version for 4PP420 but I would like to be sure that it can be the problem
Thanks!
Giovanni
Hi Giovanni,
I don’t have AS 4.0 or AS 4.2 installed on my pc, so I did a quick test with AS 4.12 and old ACP10 version similar to yours and no issue:
For the motion communication are you using CAN or powerlink? Which card do you have?
Can you try with an empty prj with just your power panel and one ACOPOS drive if you have the same issue?
In your case the issue is more related to VC4 (vcresman) and not to AR. Have you tried different VC firmware version too?
I hope it helps
Ciao
Valerio
There is no AR 4 runtime for the 4PP420.1043-75. (only PP65 AR was updated longer)
This seems a VC3 visualisation. I suggest to convert the visualisation from VC3 to VC4, probably in AS V3.0.90 and then go to AS4.
Hello Valerio,
thanks for the answers.
I am using powerlink and the MN is 3IF787.9
The VC4 versions I tried are just VC 4.0.x because I stopped to go with higher AS version when I saw the error during transfer.
Below a screenshot of the VC component. Is it VC3 or VC4?
Any ideas?
Hello Corne,
thanks for answers.
Below a screenshot about VC version.
Understood that there is no AR 4.x for AR for 4PP420.
Any idea on how to proceed with the conversion?
Thanks
Another hint @valerio.manenti
I had the problem not during rebuild but when I transfer to target. Have you try to download to a target your project?
Thanks
With this old AR version every object is downloaded seperately, so depending on a setting it could be that at some module this error comes.
Have you looked at the Objects configuration setting or tried to increase the Cyclic and B&R objects?
Hi,
just want to add some basic things here.
Error 9650 means, that “something” in the PLC tries to call a library function / function block which is not available on the system.
As this happens while transferring vcresman, it looks like that vcresman has dependencies to other libraries / system modules, which aren’t on the target (yet).
So I would first try:
- create a new blank project in AS4
- add a VC4 visualization with a dummy page or so
- rebuild this project, and transfer it to the target
- if this works without error
- check which modules were inserted in the blank projects “library” and “binary” objects section
- check if all of these modules are also present in the converted project
Sometimes, it’s also worth a try to (please make a backup of your project before!!)
- delete all library and binary objects out of the deployment table (not from the project, just from the physical views deployment table)
- trigger a rebuild all → the dependency resolve mechanism of AS should now insert all needed modules again into the named sections
- any differences to before? Any compiler / builder errors, they haven’t been there before?
Last but not least:
- after the failed transfer, there could also be a logger entry about 9650 → if yes, can you please share it, especially the information in the “ASCII data” column if there’s some information inside?
Alle of these measures won’t solve the problem I think - but at least I hope that here or there some additional error / info comes up that points into the direction what’s missing.
Best regards.
Hi @Giovanni_Boschello ,
I don’t have this panel in the office.
Based on your screenshot you are using VC4 and not VC3.
arsim for 4PP420 is available only since AR 4.x and unfortunately as Corne said there is not AR 4.x for your panel.
Please follow the next steps proposed by Corne and Alex.
In the past in similar case, in the new prj I did:
- added new empty visualization (+ I see new step transfer for you)
- imported basic elements (textgroups/Alarms/datasource), AS menu: File > Import VC resources from other prj… (+ I see new step transfer for you)
- build the prj (+ I see new step transfer for you)
- imported global common layers (+ I see new step transfer for you)
- imported as last step pages (+ I see new step transfer for you)
You know in Italy we say ‘tutte le strade portano a Roma’, maybe mine requires to claim up/down mountain 
Ciao
Valerio
I succesfully transferred (by writing to compact flash) a test project to a 4PP420.1043-B5 with a very simple VC4 visualization in AS V4.12.11 with ARI3.10 and had no issues.
This is very interesting @corne.geerts , in your sw configuration I see DataObj library and one minute ago I found one case in our Support database
same issue reported by Giovanni.
In that case, the customer solved the problem by deleting DataObj from the project and adding it again. It seems the system missed transferring that library during the initial transfer.
@Giovanni_Boschello your case is not identical to the case reported by another customer, but this dataobj library could be the problem.
I don’t see any dependency on vcresman library and dataobj library so theoretically there is no connection between them:
In general, I highly recommend using the software comparison tool (Online > Compare > Software) to check if all modules—especially the libraries—present in your sw configuration are actually installed on the target.
Ciao
Valerio
I had the same exact issue starting last week. My situation is that i have to update a project from AS2.7 to a newer version AS in my case the same AS4.0.29.87 SP.
Going through 3.0.71, 81, 90 presented its own challenges but i got through all of those and finally migrated from 3.0.90 to 4.0
The usual ACP10 errors were quickly resolved by just removing and re-adding the libraries and the project compiled fine finally. Than having big hopes i did a download and was presented the same error that Giovanni reports (Error : Error 9650 while transferring.: Library function not available (System GOT))
Ok so i created a new CF Card and put that into the plc but still no luck won’t boot by any chance.
The logger had some weird entries stating that a required library was not found on target…

(NOTE: The logger above shows a normal download not the logger after new CF! but the entry with the arPageMap was the same and some more)
The software compare window did show everything was equal to AS so everything was loaded
One thing I also noticed was this entry in the output window:

So I followed this and opened VC Editor and just opened a page and moved a text by 1px to the right and re-saved the VC. Afterwards the warning no longer showed up.
And additionally what I did was to change the AR Version from Q3.7 to H3.10!
Afterwards did a project cleanup and than a build all - transferred and now the thing is working
I am not sure if it was opening VC Editor and the AR version was not necessary but wanted to share what worked for me hopefully could also get you going or possibly helps someone else.