As I download program to the new 4PPC80.101E-10A, it goes into diagnostic mode.
On the logger it has the following error messages.
AR Version: 4.90
Hello and welcome to the Community,
From which AS version have you migrated? Which versions apart from AR have you used? Which steps have been done while migrating?
It’s hard to say a cause just from the SDM system logger screenshot, but there is some problem with “visu” installation. I guess it’s a VC4 visualization. Have you opened it while migrating the project?
The best would be to provide a system dump, but I believe you can’t do it since you’re posting for the first time.
Another option is to ask a local B&R office for support by providing them the project and system dump.
Hi @lomithap what is the status or solution of your topic? Can you update us?
closed due to inactivity without solution.