Hello!
I must replace VFD 8I74 (not available anymore) with new 8I76 type in an application made in AS version 4.2. For this version I can’t find upgrade file for 8I76. Then I wanted to convert whole project to AS version 4.12 but now I have incompatibility problem between ACP10/ARNC0 and mapp (service). In original application I have ACP10/ARNC0 version 3.18.2 and mapp 1.6.2. This is CNC machine…
Hi @Matjaz_Kopac ,
which ACP10/ARNC0 version do you need?
Based on ACP10 version you need a specific version of mapp, for example:
In general for this request you should call our Support in your area.
Ciao
Valerio
Hi!
In fact I don’t know which versions of ACP10 and mapp are compatible between each other… In AS V4.12 I can use version of mapp 1.9 (I think it is the highest).
But for the moment I solved my main problem (implementing new VFD type 8I76) with installing AS version 4.3 for which 8I76 upgrade exists. And now I came to other problems, how to set 8I76 parameters properly to correspond 8I74 settings…
ok let me install the latest version 1.9.
For what I see there are some guidelines in the Help:
=================
I have installed mapp 1.90 and now I see additional note in the Help:
Unfortunately the package Acp10Arnc0_5_27 is not available on our website so you have to call our Support for getting that version.
But for the moment I solved my main problem (implementing new VFD type 8I76) with installing AS version 4.3 for which 8I76 upgrade exists. And now I came to other problems, how to set 8I76 parameters properly to correspond 8I74 settings…
I recommend to install AS 4.12 and not 4.3
Ciao
Valerio
Hello Valerio,
I would like to reopen this case, because this issue isn’t completely solved with new Acp10Arnc. I’ve asked support for AS4_TP_Acp10Arnc0_5.28.3.1 because I have mapp 1.91. I’ve changed runtime versions and there everything looks ok. But compiler then generates following error:
Version mismatch. Module arnc0man has version or date V5.28.3 instead of required range from V5.29.1 up to V5.29.1. File: …\Binaries\STI_7\5PPC2100_BY01_000\Arnc0ext.br
It seems I need to downgrade library Arnc0ext which version I don’t have. Will lover version work in AS 4.12? Now I remembered, I asked for it some year or two ago and was quite a problem to get it. It seems I gave up that time..
I solved actual problem of exchange inverters 8I74 => 8I76 at the machine with project convertion from V4.2 to V4.3 but for the long term this is probably not a solution… We have few more similar machines made on old AS verions.
Hi @Matjaz_Kopac ,
I solved actual problem of exchange inverters 8I74 => 8I76 at the machine with project conversion from V4.2 to V4.3
always drastic solution… 
I’m looking for the upgrades, I’ll update you soon
======
no issue on my case (AS 4.12.9):
========
Have you received AS4_TP_Acp10Arnc0_5.28.3.1.exe or AS4_MC_Arnc0ext_V5.28.3.exe?
Ciao
Valerio
Hello Valerio!
Thank you for all support. Yes, I hade to do something quickly, because machine is used night and day, so I changed to AS V4.3 for a moment. In version AS 4.12 I have all upgrades OK, except I don’t have appropriate library AS4_MC_Arnc0ext_V5.28.3… I didn’t receive it yet, I’ll ask our support in Prague again.