Hi,
Where can I check which AS version my CPU is compatible with, whether it supports mapp motion etc.?
I currently have an old ‘4PP420.1043-75’ model CPU. Which AS version should I program it with? Can I use mappMotion?
Thanks.
Hi Arif,
you can check the B&R Homepage for available Upgrades / AR Versions.
You should be able to use it in any AS 4 version, since there is an AS4 upgrade. You probably only need to activate the “legacy” button at the top of the toolbox. As for the AR: the newest one seems to be I3.10. So that’s a big no for all mapp components.
Also the PP400 has limited system resources and probably couldn’t handle current AR versions or software packages as mappMotion / mappServices anyway…
For ACP10 im not quite sure which versions you can use…
Best reagards,
Marcel