Error status on X20PS9400 while updating HW configuration

Hello All,
I am reaching out to you guys this time for help regarding an error status on X20PS9400 (Power supply module for BC & internal IO supply). I am redoing hardware configuration in my project file. I am using APC910 system and the hardware configuration I am trying to build as follows:

X20SL8101 → X20DI4371 (4x modules) → X20PS9400 → X20DO4322 (4 x modules) → x20AI4622

When I am trying to add X20PS9400 after 4 x X20DI4371 modules, it won’t add with these modules.

This is the configuration I am trying to building:

Another thing which I am noticing is SafePLC is not getting online despite the face the connection to SafePLC seems fine.

Is there anything I am missing out?
Any insight on this would be greatly appreciated.

TIA

You can add X20PS9400 only to the Bus Controller bases (X20BB).

If you wish to add a power supply module between X20 modules you should use one of the following:

  • X20PS2100
  • X20PS2110
  • X20PS3300
  • X20PS3310

Regarding the Safety PLC have you checked the Powerlink Node number (dip switches) on the actual device? Seems to be set as 3 by looking at your picture.

Hi Tommy,
Many thanks for your quick reply and you are spot on! I tried to add X20PS2100 and it was letting me but in case of X20PS9400 (Power supply module for BC & internal IO supply) it didn’t which is also confirm with your guidance.
Regarding Safety PLC, yes the DIP switch of the actual device is set at position 3 as it was before in the previous configuration. Can you please guide what to do here?

TIA

Hi Syed, what is the status of your topic, can you update us?

Closed due to inactivity of author