Hello,
I have this error, with no clue how to solve it.
Also, whenever I try to Rebuild my project, I’ve the following error multiple times :

Those problems started when I installed 4.9.3.144 (from 4.9.2) with the service pack.
Do you have a solution ?
Thanks in advance,
Regards.
Is this laptop updated to Windows 11?
If so update to AS V4.12, because AS V4.9 cannot be used on Windows 11.
Yes my laptop is working with Windows 11.
No it is supposed to work on Windows 11, and have already made it running in 4.9.2.
Those are my specifications :
I cannot and won’t upgrade my project to AS 4.12. I must stay in 4.9.3.144.
oliver_D
(Oliver D)
5
I am sorry for my rather hard answer here but AS4.9 is not intended to be run on Win11
Even if it ran at a certain point it is not guaranteed that it will run with a different service pack (either AS or Win11)