I’m using the 4PPC50.101E.10A module for a project. When I reset the HMI, it starts in RUN mode. However, after I transfer the program to the HMI, the screen goes blank.
I can still see the visualization through a VNC Viewer, but the HMI itself displays the message “Unable to connect to socket.”
Why is this happening, and how can I resolve the issue?
Hello Abin,
I would expect this to most likely be an issue with how either AR or the terminal side of the C50 has its network settings configured properly. Could you provide the settings from your ETH configuration as well as the Terminal configuration (found in PLC configuration).
Also have you taken a look at the logger with all relevant modules enabled? Is there anything of interest in there?
Great. Please, if you provide a picture, it is always good to also describe what you have done and the status of your progress. Btw, you set the IP address of your terminal to 192.168.0.20, but this IP address is already used for the Ethernet interface IF2, so if you have not changed that, then now you have an IP address conflict. So set different IP address for yoor terminal e.g. xx.xx.xx.21. For VNC if localhost will not work, try to set same url you are using from external PC. e.g. 192.168.0.20:5900, format is IPADDRESS: PORT OF VNC server
Thank you very much for the help! You were right: the terminal had the same IP address (192.168.0.20) as the Ethernet interface IF2, which caused the conflict. I changed only the terminal IP to a different address (192.168.0.21), and the problem is solved. I’ll also include a short description of my progress together with any screenshots I post in the future.