First of all, thank you for sharing the screenshots and configuration steps.
We are using an X20CP0482 CPU with Bus Base X20BB67, and the project is developed in Automation Studio v6.1.1.14. We have configured the system as per the steps and screenshots you provided.
However, we would like to understand how to confirm whether Ethernet POWERLINK is properly configured and running on the controller. Could you please guide us on the following points:
How can we verify in Automation Studio that the Ethernet interface is configured correctly for POWERLINK (MN/CN mode) and that the POWERLINK stack is running?
Which diagnostics or status indicators should we check to confirm that POWERLINK communication is active?
Additionally, we need to capture and analyze Ethernet POWERLINK (EPL) communication using Wireshark.
Could you please share the correct procedure for:
Capturing POWERLINK traffic in Wireshark
Applying the appropriate filters to monitor and analyze EPL protocol data
Your guidance on these points would be very helpful.
Sub: Clarification Required on Ethernet POWERLINK ASnd / Asynchronous Communication and Object Parameters
Thank you for sharing the configuration screenshots and guidance.
Based on your inputs, we have verified the following:
The Ethernet POWERLINK status is now showing as configured and operational.
We successfully captured POWERLINK traffic using Wireshark.
The traffic capture was done via Ethernet port 2 of the X20BC0083 module.
Now, We wanted to specifically observed traffic on UDP port 3819, how it is enabling (Help me this)
However, we need clarification on a few open points related to asynchronous communication and object visibility:
ASnd / Asynchronous Communication Channel
In our current Automation Studio setup 4.12.6.106 and 6.1.1.14, we do not see any option to:
Enable Asynchronous Communication Mode
Configure ASnd channel parameters
Enable or configure ASnd (Asynchronous Send) objects
Kindly clarify:
Is ASnd/asynchronous communication automatically handled by the POWERLINK stack in this configuration?
Or does it require specific hardware support, firmware version, or additional configuration in Automation Studio?
Are there any prerequisites (e.g., MN role, interface mode, or PLK settings) for ASnd visibility?
Object Dictionary / Object Parameters Not Visible
Additionally, we do not see any POWERLINK object parameters or object dictionary entries related to ASnd or asynchronous communication.
Looking forward to your clarification on above point
Hi @Nishit ,
more than happy to help you but I ask you to create 2 new posts for 2 different questions (UDP and Powerlink object dictionary); we would like to have a post for one question.
The initial request was “How to configure Ethernet POWERLINK on X20CP0842 CPU with X20BC0083 in Automation Studio v6.1.1.14” and as you has reported your CPU is communicating with the bus coupler so I’m going to mark as solution one of my comment and waiting for the others.
Thanks
Ciao
Valerio