Installation error - AR-File can not be read

Sporadically, the error that the Automation Runtime file cannot be read appears during download or offline installation, causing the installation to be cancelled.

To solve this problem, proceed as follows.

  1. Switch to an older AR version in the project
  2. Reinstall the desired AR version via [Tools->Upgrades].
    Set the filter to and select the Checkbox [Show upgrades alreday installed]
  3. Switch back to the desired AR version
  4. Restart the installation

With this procedure, the error can be rectified and the project can be reloaded with the desired AR version.

3 Likes

I just had the exact same issue with AS4.12, APC3100 and AR J4.93.
Restarting Automation Studio solved the issue for me!

Update: Just had the same issue again after fiddling around with git. (Did some checkouts and merges)

Best regards!

cool,thanks for that :slight_smile: