Hello, I’m Choi.
Is it possible to set the IP bandwidth of Ethernet and PowerLink to be the same?
for example,
X20CP0484
ETH(IF2) - 192.168.1.199 (enter IP address manually)
PLK(IF3) - 192.168.1.200 (enter IP address manually) *Operation mode - Ethernet
When I set ip address with same IP bandwidth, error occurd..
Thanks
Hi,
ethernet interfaces have to be in different IP subnets.
Because if not, the IP stack would not be able to decide, trough which physical interface a IP packet has to be sent to reach the receiver of the packet.
That’s the reason why you get an error when trying to configure multiple interfaces to the same IP subnet.
Best regards!