Hi everyone!
I’m currently facing an issue during the conformance testing of a third-party Powerlink control node using the Open Conformance Tool V2.1.0. Specifically, I’m encountering a failure in the test case related to writing an object.
![]()
we adjusted the high limit value (100µs) for object 0x1C14 according to the newest specification to pass the testcase “write OD highLimit” from the Conformance tool.
However, the tool tries to write a much higher value (12.5ms) during the Bootup and NMT State tests.
We suppose that the tool writes these large values, because of the high jitter caused by running it on Windows OS.
Has anyone else experienced a similar issue or have any insights on how to resolve this? Any help or suggestions would be greatly appreciated!
Thanks in advance!