LIN bus - A low-cost communication bus for mobile vehicles

Dear Community,

Let me say a few words about a lesser-known communication bus that we recently implemented. Its name is LIN. The LIN bus, together with the CAN bus, is one of the most widely used buses in mobile vehicles.

Key Features

Some advantages of LIN compared to CAN are:

  • Cost-Effectiveness
  • Reduced Wiring
  • Lower Power Consumption
    see more …

Required AS upgrades

Use cases/Demos

The Getting started section of the CpLin library help provides 2 examples of using the bus:

  • Control of a rocker switch
  • Control of an ultrasonic parking sensor

QnA

  • What version of AS is supported?
    • The library can be used in both AS4 and AS6.
  • Do I need an extra license?
    • No, you do not.
6 Likes

If you’re curious about the LIN bus, feel free to ask any additional questions :slight_smile:

Dear @vancurar,

Is this protocole likely to be available for X20 configurations soon ?

Thank you for your support,
Best Regards.

Dear Alexandre,
the LIN communication protocol has been implemented for our X90 PLCs and as far as I know there are currently no plans to make it available for X20 system.