Looking for Automation Studio V2.5.1.17 and Automation Runtime V2.35 (System 2003 / m68k)

I’m maintaining an existing plant based on the B&R System 2003 (m68k). The PLC project was created and last saved in Automation Studio V2.5.1.17 with Automation Runtime V2.35 (library set V0235). CPUs in the installation are CP474 and 7CP476.60-1.
I need to open and service this project, but the in-app upgrade download no longer works for AS < V4.6 (TLS issue), so I’m trying to obtain the setup files another way.

I’m looking for:

Automation Studio V2.5.1.17 setup (or the nearest 2.5 build, e.g. V2.5.2.108)
Automation Runtime V2.35 (V0235) package, so the target runtime matches what’s flashed on the CPUs
If needed: the hardware upgrade package for the 2003 / m68k target

If anyone has these in their local …\BrAutomation\ASxx\Upgrades folder, or knows a working download/manual-upgrade link, I’d really appreciate it. Please reply here or send me a private message.
Thanks a lot!

Hi @AndreySilin ,
Welcome to our community!

Have a look at this post (same answer for your AS 2.5.1.17):

Ciao
Valerio