Is the PC2100 still available, or is there a replacement with exactly the same specifications and dimensions as the PC2100?
Hi,
please get in contact with our local partners to arrange for repair and/or replacement parts.
The 2100 is still an ongoing product, see Automation PC 2100 | B&R Industrial Automation
Link to list of subsidiaries / partners: Locations | B&R Industrial Automation
Best regards
5PPC2100.BY11-000 this type still ongoing?
Please consult the links I provided
New link since it’s a PPC not an APC: Panel PC 2100 multi-touch | B&R Industrial Automation
the xPC2100 is still available and supported but will soon enter its ‘classic phase’ which means it is not recommended for new projects.
the xPC2200 is the natural successor.
But as Michael mentioned: contact your local B&R partner what they recommend.
the customer send me this picture
This is a customized device. You will need to contact Mettler - Toledo.
where can I contact?
can I get the model equation? from its almost identical shape and specifications
If you’re looking for spare parts, you should buy identical parts. PPC2100 is still possible to buy.
Looking for replacement of pc2100 - #2 by michael_w.
If you would like to update to PC2200, you would probably need more (software, knowledge, etc.). For this, you must contact the company that delivered it. You can find the contacts using Google.
That is all we can do for you. If you do not have anything else to discuss, let’s close this topic.
I sent the following photo if you can check it?
cant you check sir? this customer waiting this answer
Answer 1:
Answer 2:
Looking for replacement of pc2100 - #10 by kovarj Looking for replacement of pc2100 - #5 by christoph.hilchenbac
Summary:
Sorry, nothing else to add.
So the picture I sent is correct that it’s a PC2100? or not? because it looks different
Panel PC = PC + panel. So, yes, in your picture, the PC part is visible. From the model number you sent previously, we already told you that this is a PPC2100.
I was given a photo of my customer like this, to see which part of the CPU type is it?
because I’m a little confused
For hardware details and ordering spare parts, Community is not the right place. For this, you need to contact your local B&R office. As it was already mentioned in the past, your set has 5PPC2100.BY22-000
What you have is a preconfigured set and it consists of the following parts:
Still you have to contact your responisble B&R office for repair or replacement parts
If I replace my PC with this type, is it possible?
5PC9:212660.003-02
I do not think so as this set seems to be an APC910 which is not compatible with the one you have
Please contact your B&R office !