Mapp Framework 6, release candidate testing - No AuditTrail content?

Hi,

There is no Audit content of mapp Framework for AS6.5?

Also as i had mentioned before, If you can add a example to the Mapp Framwork about the database,

That would be a great help.

Thanks anyway, i will continue to test FW6 !

Hi, @jayD, thanks for the feedback.

  • Audit content is still part of mapp Framework 6, but I can see that it is not present in the importer, is this what you are missing? Because this is obviously a bug Im going to report.
  • Discussion about mapp Framework 6 extension (or redesign, e.g. link) will be the next possible step.

Jaroslav

Understood, and my sincere thanks!

I have sent you new release candidate, have you received it? What is status of your testing, any new findings?

I have received the latest version and am currently testing it. Should any issues arise, I will promptly provide feedback. Thank you.

Would be great if you provide me final feedback till end of this week, so we can close this version and release offical version.

Subject: Issues with User Management and Audit Trail (Possibly AS6.X Related)

Hello kovarj,

So far, I have found that functionalities such as Recipes, Axis Control, and Reports are working properly.

However, I am experiencing some confusion regarding User Management and the Audit Trail. I suspect this might be related to AS6.X?


:magnifying_glass_tilted_left: Issue 1: Default Login Without User Interaction

I noticed that I can perform all operations without explicitly logging in as any user.
Upon checking, I found that the system automatically logs in a user named SystemUser by default.
I believe this is a bug.


:clipboard: Issue 2: Audit Trail Problems

  1. Incorrect Logging of Login/Logout Events
    Whenever I log in as any user, four audit records are immediately generated.
    Normally, there should be only one record for a successful login.
    This behavior seems incorrect.

  2. Wrong Operator Recorded
    For any audit-relevant operation performed by any user, the operator is incorrectly recorded as the default SystemUser.

  3. Audit Configuration Not Effective
    The options in the Audit Configuration do not take effect.
    For example, when I click the Save button, the file is not correctly recorded.
    As a result, the Export Archive function is also not usable.


:globe_with_meridians: Issue 3: Language Display Problem

After switching the interface language to Chinese, the Audit Trail window is displayed in German.
However, the Chinese TEXTS are correctly configured.
This is very important for my work.


:speech_balloon: Final Note

I would like to report more bugs as I continue developing with this platform, and I plan to submit them to the community gradually.
Unfortunately, I don’t have time at the moment to do so.

Thank you all.
Issue 2-1


Issue 2-2


Issue 2-3

Apologies for the delayed reply due to the time difference.
Please see the feedback above

Hi @jayD,

Thanks for the report. We have checked all of them, and in the end, I have decided to create a new page in the visualization with a focus on changes caused by migration. Some of the points are features, and there is also a bug in mapp services we have found thanks to mapp Framework testing.

Regarding the audit text, you are right. The Tmx file does not contain translation. Do you think you will find time and translate it for us? It’s this file:

Would be great to have it this week. :slight_smile: just let me know. Thanks

Hi @jayD.

I used automatic translation in the end. I need to release mapp Framework 6. Thanks for your help so far. :slight_smile:

Sorry for the delay! I’ve been offline for the Spring Festival break. I’m back to work now and excited to see the next version!