Mapp View : change dynamically the port 81 to 82 for example

Dear All,

I would like to change dynamically the port 81 to another one (82 for example) by the process once time during start-up but I don’t see any information on the Help file.

Do you have any idea ?

Thanks a lot

Sebastien

Hi Sebastien, this is not possible. What is the usecase for that?

Hi Sebastian,
if you would set a Rule like this:

UPLINK:TCP:82>DEV1:10.0.0.41:81

then you should have access to the mappView visualization of the second controller with IP10.0.0.41 via the IP address of the Site manager’s Uplink port, Port 82

Regards
Oli

Dear Oliver,

Perfect, I tested it and it’s running !

THank you.

Sebastien