Mapp View Issue in AS6 Migration

Migration from AS4.12 to AS6.

Currently using AS6.5.1.7

AR-6.5.1

Mapp View - 6.6.0

All the required upgradations are completed for AS4.12 to AS6. While simulation testing, In mapp view all type widgets are not displays properly. Eg. In Numeric pad its Shows XX, not able to enter values or not able close the numeric pad. Same type errors occurs for all widgets used in mapp view. Is AS4.12 mapp view working fine without any issues.

Hi Thiyagarajan,

i would recommend checking the OPC UA and Access and Security Setting.

With AS 6 a lot of “unsecure” connection options are disabled by default. For example connection via the “Anonymous” User.
If the mapp View Client cant connect to the OPC UA server correctly the XX will show up in the outputs.
Also the Automation Studio Logger should show Entries regarding the issue in the Connectivity and Visualisation categories.

Hope this helps

1 Like