MappView and 5PPC2200

Please advise me how to set up ppc2200 to display mappView visualization?

This is the terminal setting. But I can’t find this setting for ppc2200…

If you are using a 5PPC2200 as a mapp View client all of these settings are done with in tine General Purpose OS (GPOS, i.e. Linux or Windows). Generally this is done with a startup script or setting of some sort, i.e. bypass or automatically logins and launches a web browser to the mapp view server URL. There are guides on the general internet on how to setup windows or linux to do this sort of thing.

The Terminal OS like the one on the Power Panel T panels isn’t available for the PPC2200. It’s only available for PPC3100, PPC900 and future Panel PCs at those performance levels. (i.e. the PPC2200 isn’t anymore powerful than the T80.)