How to display Mappview screens in 5AP1120.1505-0000 PPC.
Web browser needed for browsing the Mapp view screens but OS not there in this PPC.
What is procedure for installing OS & Browsing the Mapp view screens.
Please help us. little urgent
How to display Mappview screens in 5AP1120.1505-0000 PPC.
Web browser needed for browsing the Mapp view screens but OS not there in this PPC.
What is procedure for installing OS & Browsing the Mapp view screens.
Please help us. little urgent
If you have a serial number of the system, you could look up on the B&R website in what configuration this panel was delivered and also with which operating system.
Hello,
5AP1120.1505-000 is not a PPC, it is a 15 inch display panel which is attached to some PPC.
If you expect to get help from the community, you would need to at least provide basic information about the model name of the PPC and the OS type and version that is currently installed on it.
One way of doing that is to follow a suggestion by @corne.geerts (above) and share the details here.
Thanks and Best Regards,
Alexander
Share with us serial numbers or take a picture from the backside of your hardware, ensuring that the serial numbers and model numbers are visible. If you have only AP=automation panel, you would need PPC unit as well. But without detailed info we can not really help you.
Since there is no GPOS included in this set, it is either an ArEmb system or CU used to install their own GPOS system. The original description mentions that the OS is missing on this target. In this case, you need to purchase a license for the hypervisor and respective GPOS, modify the configuration in your project, and install both GPOS and the hypervisor.
Thanking @kovarj for the information and recommendation, may I suggest that since the 5PPC2100-BY22.000 model has only 2GB of RAM, another possible way would be to use a Windows OS and ARwin.
But I can’t say much about the license differences. Perhaps ARemb license (which should be included with the system on a HID dongle) would work with ARwin. I’m not sure…
Jaroslav, could you please comment on this?
For a hypervisor system, 2GB is the minimum requirement. See this link. So, for a simple application with Linux GPOS, you might still be able to use a hypervisor. But, it’s hard to say without knowing your specific requirements. ArWin has been obsolete for a long time; I’m not sure if you can still install or use it. This is a question for other colleagues in the Community or BR support. From a licensing perspective, ArWin and ArEmbedded are two different products and thus not compatible.
Jaroslav, thank you very much for the clarifications! I did not know such details regarding ARwin…
Hi All,
Thank you all,
Installed Linux & Hypervisor its working well.
Great! Glad to hear that you solved the problem. Please mark one of the posts by Jaroslav Kovar (@kovarj) as a solution.