I have been doing some testing with my BnR Panel PC 900 and a domain controller to implement Active Directory user management on the Panel PC’s users.
I have everything connected and the users I have implemented on the DC side work. My goal is to use local users and users authenticated by the DC, so I have the setting on MpUserX set to “Local and central”. What I find is that if the DC is powered on and connected, all users can login and work fine. If the DC is powered off, the DC users AND the local users are no longer able to login and use the panel.
Hi Alexander,
I have no idea about the caching. I’d expect this not to work this way.This you should check with local support, as well as the automatic timeout setting :).
I’d also recommend you to upgrade to the latest available version for mappServices which is 5.24.6.
It is behaving as expected. When the DC is on both local and central users work. If the DC is off then only the local users work.
I have observed a little weird behavior in that it seems when the DC goes from on to off, it takes the Panel PC a minute or so to figure out this happens. During this time I have also observed that neither local or central users is able to login until the Panel PC “finds out” that the DC is off and then local users work. I’m sure with some diagnostics and visual cues this can be cleaned up.
All in all its working, thanks to Jan VDW for pointing me in the right direction.