MC_BR_RegMarkCapture001 Usage in mark correction for cutting

Dear All,

I need help in using MC_BR_RegMarkCapture001.

Which mode and parameters should be used if I want to use the mark as a trigger and cut offset as the distance between mark and cut of a continuously moving axis with camming to master virtual axis.
Earlier I was using mode as FIRST TRIGGER + INTERVAL, but it gives me large correction values when the cut offset increases heavily. I think I am doing some error in calculation, or mode selection. So i need basic understanding for the same.
Can anyone explain the modes, parameters and calculating reg mark position for the requirement.

Do let me know in any need.

Thanks in advance

Hi @bhaglanid ,
to be honest when I worked with printmark correction PLCopen function block was not ready yet so I implemented my solution with SPT.
In the help I think we have an example that described step by step what you have to do:

I recommend to do more traces to identify the cause of your issue.
Without any data/traces it’s hard to help you.
When I studied my first printmark correction in the lab, it was not a project for one day so it took a while to understand the meaning of all parameters.

Ciao
Valerio