MpAxisBasic with stepper motor and X20SM1446-1

Hi,

I am using the MpAxisbasic FB to control a stepper motor : type 80MPH4.500S114-01 in combination with an X20SM1446-1 module. Everything seems to work fine and I can control the motor with “MoveAbsolute” (for example). The motor runs nicely to the preset position and also stops when on position and gives “InPosition” back from the FB, but I get no feedback “MoveDone” from the FB.

Does anyone have any idea why this is not coming back from the FB?

Regards,

Hi,
are you resetting the “MoveAbsolute” input immediately?

According to the Timing diagrams “MoveDone” is reset when “MoveAbsolute” is reset:

Indeed, that’s where i made a mistake.
Thanks!