Multi Axis ACOPOS P3 DC bus

ACOPOS P3 2-axis modules or 3-axis modules like 8EI8X8HWD10.XXXX-1 or 8EI8X8HWT10.XXXX-1, Does per axis in same one ACOPOS P3 share DC bus?

yes, sure. There is only one connector for mains.
What is the background of your question, please ?

Thanks for the answer.Here is the background.
There are two rubber roller next to each other.There is friction between them.They driven by different motor 8LSA56.​ee030ffgg-3.One roller is always running slower than another one .
i think it don’t need braking resistor if 8EI8X8HWD10.XXXX-1 share DC bus

Got it.
Yes, this is the basic concept behind P3. All axes of one drive share the DC bus.