Difference between acopos multi and P3?

Please tell me Difference between Acopos Multi Drive and Acopos P3. I mean in which kind of applications require Acopos Multi and which require P3?

Im not expert: But our AI CHat returns to me this: Both ACOPOSmulti and ACOPOS P3 are drive systems with multiple technology-specific functions. ACOPOSmulti functions include point-to-point movements, electronic gears, cutting units, electronic cam profiles, flying saws, line shafts, and CNC. On the other hand, ACOPOS P3 is a scalable drive system with a wide range of functions designed for controlling various types of motors. The choice between the two depends on the requirements of the application. ACOPOSmulti is suitable for applications that require advanced motion control functions, while ACOPOS P3 is ideal for applications that require a scalable drive system for controlling various types of motors.

can any expert from community check it? :wink:

Thanks Jaroslav, We had an application of Universal line for Filling and Capping in between using ACOPOS 6D for Transfer mechanism. I think ACOPOS Multi would be preferred one here!

Shortest comparison I can make:

ACOPOS P3: Standalone drives with up to 3 axes (per drive), rated currents ranging from 2.2A up to 44A

ACOPOSmulti: Modular system, 1 or 2 axes per drive, rated currents ranging from 1.9A up to 200A; can send excess amount of energy (e.g. during braking) back to the power grid

Generally speaking I recommend looking through both product pages to get a feeling for eeach product group

And since I was typing my reply, @kovarj sent his. I must disagree on the comparison of the AI bot. BOTH drive systems allow for the same range of movements, but our marketing sites for both drives list different things (or some not at all) so a direct text comparison like the AI did is not giving you the real picture here.
See
https://www.br-automation.com/de/produkte/antriebstechnik/acoposmulti/
which lists those things like “flying saws”
vs
https://www.br-automation.com/en/products/motion-control/acopos-p3/
which doesn’t

Also, both systems are scalable, seen by the fact that there are subpages linked on each product page using exactly that keyword :slight_smile:

cool. Thanks Michael. I wanted advertise our AI conversational help, because this is excatly the question I would ask it. But you always (as with any other AI chat) think about the result. But general overivew + links to AS Help link very good. So can be used by people I would say.