Hi everyone,
I’m working with a legacy B&R controller – model 7CP476.60-1 (System 2003).
I’m using Automation Studio 2.6 and trying to back up an existing system and move it to another identical CPU.
Here’s the problem:
The old controller runs on SW 2.32
The replacement unit has SW 2.40
When I try to load the project files onto the new controller, it boots into Service Mode and all tasks are in STOP
I’m guessing this is due to the Runtime version mismatch
Unfortunately, AS 2.6 only comes with Runtime versions starting from 2.40 – I don’t have 2.32 in the system.
If anyone has a copy of Automation Runtime SW 2.32 for System 2003 or knows where I can get it, I’d really appreciate it.
Thanks a lot in advance!