OPCUA TSN not working

Hello everyone
I’m currently trying to get two 4PPC80’s to communicate in real time. I checked and these should be able to perform TSN and VLAN configurations. I followed this guide and rechecked multiple times. Both projects have OPC UA FX and C/S in the runtime Config. The TSN switch is configured as shown in the guide and i tried different settings, while trying to get it to work. Here is it now:

Both projects have certificates and ssl configurations done right. Both are in the PTP Mode “slave only”. System timer and resources are configured. Publisher and Subscriber are configured like this:

The Client has the binary imported, the writer deleted and the same VLAN settings.
OPC UA Client/Server and the defaultView is enabled on both. If I disable VLAN the client get’s the data but to my understanding this isn’t TSN anymore then. The Logger entries of both look clean no errors no warnings since last restart. On the server program i set the variables only and the client just has a if-clause that triggers if the Bool is true or the Int is greater than 0. Both programms are in Cyclic #1.
Could someone look through this and tell me what could be wrong?
Thanks for all the help
Nick

Hello,

it looks like the community does not jet have a lot of TSN Experts active.

My First check was that C80 is supporting TSN and this is TRUE.

As some days are already over, did you get in contact with your local B&R Support?

Greetings
Michael

I asked a colleague to help there. He reviewed the screenshot and has not found anything. The example is quite huge and needs detailed investigation of the project itself, so nothing we can do here. So I agree with Michael that official support is probably the easiest option there.

1 Like

Hi, is it possible to provide the project? Then it would be easier to check.
Which version of the TP are you using?
Do you get Connectivity logger errors?

AR is on Version 6.6.2, OPC UA C/S is on 6.6.0, OPC UA FX is on 6.3.1. The Logger is after a warm restart clean without errors or warnings.

Thanks for looking at it i will try to get in contact with the official support.