Hi Oliver, I hoep you would be so kind as to send on teh PG2000 software to me in private message please. I have a customer with a B&R 7CP474.60-1 Rev.D0 2003 controiller that has lost its program
Hello @rayg123
Sure… I will send you PG2000 but I would like to mention that a CP474 could also be programmed with Automation Studio
So if you have a backup of the original software it is either PG2000 or AS
Still you will get a PM with the latest PG2000
EDIT: Seems as the forum software gives an error when trying to send a PM. I will try it a bit later to send you a PM
best regards
Oliver
it seems it is a D-DOS program. Wuold that work on AS?
You cannot open PG2000 projects with Automation Studio (or vice versa)
It is correct that PG2000 is a DOS program and therefor you need native DOS or Win95 but Win95 might give you troubles with the online connection and therefor I suggest native DOS
Bonjour Olivier,
Je Lis souvent vos message et conseilles, Merci pour les infos
J’ai besoin du logiciel PG2000 v2.44. Pouvez vous l’envoyersvp
Merci Beaucoup
Cordialement
Hello Oliver,
I am looking for the PG 2000 software and the manual for reloading the program of an old PLC.
Can you please send it to me?
Best regards
Eric
Hello Oliver, I am need of PG2000 to down load a project to an old generation machine with 2005 series hardware. Could you please share me the link for PG2000 latest version? I have Win XP laptop with true RS232 and DOSBox with me.
Hello Oliver, I am need of PG2000 to down load a project to an old generation machine with 2005 series hardware. Could you please share me the link for PG2000 latest version?
Hello and welcome !
Sure - I will send it to you
Hi Oliver.
Could you please send me PG2000 software?
Hello Oliver,
Could you please send me the Prosys software ?
We are working with a B&R M264 PLC in the field.
CPU model: M2NTCP63 (NTCP63)
Due to the age of the device, the serial number label
is missing or no longer readable.
We need the B&R PROSYS (Programming System) software
to connect to the PLC via RS-232 and to get in
the existing program.
Could you please support us with the appropriate
software version and documentation?
Thank you in advance.
Hello Oliver,
Could you send me the PG2000 and Prosys software?
Thanks in advance!
Rik
Dear Rik Engel,
The link is here
I joined the upgrading of the VFFS Hayssen sandiarce machine the year 2009. I hope you have a need thing.
BR