We have an old Power panel 4PP220.0571-65 and it’s broken. We are going to buy used panel from Ebay. Panel model is the same but Version, HW-Layer, OnBoard AR and SMC Version are older in panel witch we are going to buy.
Will the application on the flash memory card work on the device I am purchasing?
The Power Panel 4PP220.0571-65 is a model with Compact Flash. All the necessary versions are located on the Compact Flash of your actual machine, and those version will be installed automatically when you connect the Compact flash of your machine on the new Power Panel, during the first boot up.
The only important thing here is that you must be sure it is the exact reference, 4PP220.0571-65 and in the case you have an interface on the SLOT1, this must also match.