Ok this is not the logger. This is output window with messages from compilation. You have to obviously enable OPCUA server by the way. But this is not the reason why you can not connect to mappView server. For opening logger, you have to connect with Automation studio to the target and select in top menu option OPEN-> LOGGER. Once your are connected with your AS to the target using ETH1, try to establish connection to mappView server using 192.68.10.2:81 from any browser on your local PC or open sdm in browser using 192.168.10.2/sdm, there is also option to see logger. If this is running, you can return to browser on your panel and try connection using ethInternal.