Dale_Webb
(Dale Webb)
December 3, 2025, 9:07am
1
Hi,
Struggling to get the Config, Status, Diag bytes from Beckhoff coupler BC3150 to come into the Master as the correct Datatype.
What I should be getting from each Slave device:
16 Bytes Configuration
16 Bytes Status
16 Bytes Diagnostic
What I am actually getting is a single BOOL for each. Is there a way of changing datatypes and adding mapping here?
all the process mapping is working great, would just be good to get this extra information.
Any help would be greatly appreciated, Thanks
Dale Webb
Hello,
diagnostic data of Profibus slaves must be read using a function block. You cannot enable this to show up in the IO mapping.
In case of a IF1061-1 it would be nxdpmGetDiag()
best regards
Oliver
Dale_Webb
(Dale Webb)
December 3, 2025, 9:53am
3
Hi,
Amazing Thanks, I take a look.
We are using APROL 4.4 p6, will this information be usable in CAEmanager?
Dale Webb
You are welcome !
Regarding Aprol I cannot give a 100% statement - I never used it. Sorry
But I would say that standard B&R libraries are also available here
Dale_Webb
(Dale Webb)
December 8, 2025, 10:55am
5
I am able to get the Library into APROL,
Trying to get diagnostic data from all the slave devices such as module states and error codes,
seems to be quite a few function blocks in the AsNxDpM and AsNsDpS. Anyone have any experience using these Libraries?
I would like to get the Individual Slave state, if it is in error etc. Also the individual KL modules on that slaves state if possible?
Any heads up would be great,
Cheers Dale Webb