If a factory new profinet slave device is connected, I want to check the device and vendor ID and when it is matching with the pre-configured device in the device table of DTM Configuration it should be able to set this values programatically.
There are a few functions in the AsNxPnS library, but only for the X20IF10E3 slave module.
I also need the possibility to reset the slave device again to factory reset.
Or how can I execute ProfiNet DCP functions over X20IF10E1?
Hallo Rainer,
the dynamic configuration protocol cannot be influenced from within the application. The IF10E1-1 can only establish communication via the dynamic configuration protocol with devices added to the hardware tree.
Gruss
Stephan