Question about interpreting BRAKE_MODE parameter (ID 90) on ACOPOSmicro 80VD100PD.C000-01

Hello everyone,

I’m working with an ACOPOSmicro 80VD100PD.C000-01, and I have a question regarding the interpretation of the BRAKE_MODE parameter (ID 90).

Since this device only has one digital output for brake control, I decided to use it for motor 1, and for motor 2, I’m controlling the brake via a PLC digital output.

To eliminate the “low brake voltage” error for motor 2, I set the BRAKE_MODE parameter to 2, and the error disappeared. However, I’m a bit confused about the interpretation:

  • I understand that BRAKE_MODE is a 9-bit bitfield, and the value is entered in decimal.
  • According to the documentation, decimal 2 corresponds to Bit 1: CMD_BRAKE at "Controller on" enabled.
  • However, I assumed that to disable brake monitoring (and avoid the error), I should activate Bit 2: Control monitoring off, which would be decimal 4.

So my main question is:

Am I interpreting the BRAKE_MODE bitmask correctly?
I f I enter the value 2, am I really activating Bit 1 and not Bit 2?

Any clarification or reference would be greatly appreciated to better understand this configuration.

Thansk in advance.

Regards.

HI there,

this is just pure numbers in different representation. If you do not feel comfortable interpreting any of those manually, the windows calculator can do this for you:

Step 1: Set it to programmer mode


Step 2: Click the icon to switch to binary view

Step 3: Click all the bits you want to set

You’ll see that setting only Bit 2 is decimal 4, so 2 is Bit 1, 1 is Bit 0 and so on…

So if you set it to decimal 2, yes, you din’t disable control monitoring.
Also I am unsure if you can even disable the low voltage monitoring that way.
To disable a brake, set all the parameters of the brake (MOTOR_BRAKE_…) to 0, then the drive should not attempt to open/close it for you