During compiling of an (older) project, I get every time the error “runtimeframe start-up failed”
For this project I’m using AS4.5 with AR J4.25. (another AR version gives the same error)
How to solve this problem?
During compiling of an (older) project, I get every time the error “runtimeframe start-up failed”
For this project I’m using AS4.5 with AR J4.25. (another AR version gives the same error)
How to solve this problem?
I have never heard of such an error. Could you attach a screenshot of the error message ?
Sounds like J4.25 is not installed for ARSim
Basically every AS installation comes with certain AR versions. “Automatically” no other AR will be installed and this needs to be done by the user
In your case the AR seems to exist but it also seems that some files are missing - similar as some files were not correctly installed or available
probably it has to do that J4.25 is developed for AS4.2 ? Think have to update it to 4.53 and see if it is solved
J4.25 is not part of AS4.5 but it still should work
Nevertheless both versions are outdated since years
Great to hear ! Thanks for the feedback
Unfortunately, the problem has still not been resolved. The previous issue actually consisted of two problems (the simulation also did not work, but that has been resolved).
But I discover other problems, and I think they are related to each other.
In a project in AS4.6 I get with compiling the error: “RuntimeFrame start-up failed!
![]()
In AS4.2, when I go to tools > Update DTM Catalog I get:
in AS 4.5, AS4.6 and AS4.7 Tools> 3rd-Party device manager:
In AS 4.12 there are no problems, the device manager is working there
Anny Idea what can be the problem ??
Is this Windows 11 ? If yes then it might be the problem as this is not supported. Such old AS versions only run on Win10
It’s windows 11, but it has always worked before
FYI, I had exactly same issue today. Then I check the DTM log file,found out that it was a XML parser error. After reinstall MSXML4,problem solved.