SafeDesigner project dynamic password for CRA?

Dear forum users,

I have a question regarding mappSafety and Safety project password management.

I use a single machine configuration that is deployed to multiple machines. Currently, all machines use the same Safety project password. However, due to Cyber Resilience Act (CRA) requirements, each machine should have its own unique password.

Is it possible to make the Safety project password dynamic, for example by assigning it from a variable during installation or commissioning?

Before migrating to mappSafety (sfDomain), I was able to set the password programmatically after formatting the SafeCPU using the asSafety library. For example:

example cyclic Code:

lRemoteControlCmdTypeV1.Command = safeCMD_ENTER;
lRemoteControlCmdTypeV1.Data = safeCMD_SK_PW;
safeRemoteControl_V2_0.Execute = TRUE;

During initialization, I could set the Safety CPU password with:

Example init Code:

strcpy(ADR(lRemoteControlCmdTypeV1.Password), "password");
strcpy(ADR(lRemoteControlCmdTypeV1.NewPassword), "password");

This allowed me to assign a unique password to each machine automatically.

With sfDomain, we currently log in using the System Management user role, and we have already implemented a dynamic, machine-specific login password for this role. However, when connecting to the Safety application, we still need to use the same standard Safety password on every machine.

Therefore, I am looking for a way to make the Safety password machine-specific as well. Is there any mechanism in mappSafety/sfDomain that allows the Safety password to be configured dynamically during installation, commissioning, or first startup?

Has anyone implemented a CRA-compliant solution for this use case, or can recommend a best practice?

Thank you in advance for your support.

I am using one configuration for all machines and machine option variables to configure machine-specific Safety and non safety functions. Maintaining a separate Safety configuration for every machine would significantly increase development, validation, and maintenance effort

Hello Marcin,

for mapp Safety we differentiate between 3 passwords:

  • SafeDesigner project
  • Safe Key
  • Safety Admin User

For a running machine only the Safety Admin password is relevant as you login with this one to update/confirm/etc. the safety application.
The other two are only for the development/commissioning and are therefore not used for a machine in the field.

The password you have been able to set before was the Safe Key password.
Mapp Safety does not require this one to update the safety project with the predefinded HMI or the SfDomain library.

Best regards,
Christoph