Safety designer - Not able to find the UI menu and POU close button on version 4.4.1.0

The highlighted options and POU close button is missing in the safe designer UI I tried

  • Changing the resolution
  • Reinstalling the version 4.4.1.0
    but did not get the options back any advice or suggestions to have them back.

Thank you in advance.

Hi @harshagowda0707 ,
Click on Project → Options:

Select all Toolbars:

Ciao
Valerio

Hi Valerio,

Unfortunately I don’t have the project option also the entire line of options are not present.

Hello @harshagowda0707 ,

with the key shortcut “CTRL+0” you can open the “Options” and try “Reset”.

If this doesn’t help, I would suggest that you import the attached registry key in the Windows Registry.

ToolBar_SD441.zip (793 Bytes)

br Christoph

Enabling this worked for me.

Thank you for the support.