Safety Lodger Invalid mapping

Here I have an error ID 122909 Entered by DI SafetyLogger Description is invalid mapping, truly appreciate for any idea to solve this error.

Best regards,
David

Hello David,
welcome to the B&R community!

There should be this information in your AutomationStudio help:

Error number: 122909 (16#1e01d)

Error code
GFW_MAPP_ERR

Short text
Invalid mapping

Error description

There is a difference between the data channels in the safe application and the data channels of the bus system

Info1= first invalid mapping object 0x00XXYYYY X … Subindex Y … Index

‘binary data’ offset information
binary data[16..15]: Info0
binary data[20..17]: Info1

Trouble shooting suggestion
Ensure that the safe and non-safe application match together.
Compile and download the non-safe application.
Compile and download the safe application.

With some versions this problem happens if there are unused (that is: no channel mapped) safety modules in the SafeDESIGNER project.

Are the “Trouble shooting suggestions” not helpful in your case?
What versions are you using?

regards
Roman

Truly deeply appreciate for your reply and details informations. It help to understanding more on BnR which I am very nubie.