Script for Upgrades Install

Hello

is there anyone that founds a way to install upgrades automatically via script?
I mean lookup to hw file, then download script packages from B&R site and install packages

With the lookup logic from hw file I’m ok

Many thanks in advance

Marco Sartori

Hi,

you can use the *.exe installers with command line parameters.
Unfortunately they are not documented for HWxxxx.exe installers.

Automation runtime installer command line parameters

but I tried a little and put an example in this post: Unable to add motor from hardware catalog - #4 by christoph.hilchenbac which worked well on my PC.

Regards,

This is the right link I think:

B&R Online Help